Skip to content
LAPP Indonesia
Spend Rp 1.200 more for FREE shipping.
FREE shipping will be applied at checkout

Your cart is empty

Continue shopping
0 Cart (Rp 0,00)

Cables and Connectors from One Source: Why Integrated Connectivity Matters

Sourcing cables and connectors from a single manufacturer provides matched components designed to work together, single-source accountability when issues arise and simplified procurement with one point of contact. LAPP is unique among major industrial connectivity suppliers in engineering and producing both ÖLFLEX® cables and EPIC® connectors in-house, ensuring optimal compatibility and unified technical support across ASEAN.

Industrial connectivity procurement typically involves three or more suppliers: one for cables, another for connectors and a third for cable glands and accessories. Each supplier provides components that meet individual specifications, but nobody guarantees how those components perform together. When a connection fails, the cable supplier points to the connector and the connector supplier points to the cable. This article examines why single-source connectivity eliminates these problems and how to evaluate whether your supplier can deliver on that promise.

What are the benefits of single-source connectivity?

Single-source connectivity means procuring cables, connectors, cable glands and labelling from one manufacturer who designs these components to work as a system. The benefits compound across procurement, engineering and operations:

Guaranteed compatibility. When the same manufacturer produces the cable and the connector, mechanical fit is verified at the design stage. Cable outer diameter matches the connector’s gland range, conductor cross-section matches the contact’s crimp barrel and sheath material is compatible with the housing seal. You eliminate the tolerance stack-up risk that appears when combining products from different manufacturers.

Single-source accountability. When a connection fails—whether from a manufacturing defect, installation error or environmental degradation—one manufacturer investigates, one manufacturer provides the replacement and one manufacturer covers the warranty. No cross-supplier finger-pointing and no delays while two companies debate responsibility.

Unified technical support. Your design question—“Which cable works with this connector in a 40°C drag chain running at 5 m/s?”—gets answered by one engineering team that understands both products. You avoid the back-and-forth between cable and connector technical departments that delays machine design.

Simplified procurement. One vendor code, one purchase order, one delivery schedule and one invoice per connectivity package. For OEMs building 50+ machines per year, this consolidation reduces purchasing overhead significantly.

Consistent documentation. Test certificates, datasheets and compliance documents follow the same format and reference the same standards. Your quality department processes one documentation package instead of reconciling documents from multiple suppliers.

Why does matched cable-connector design matter?

The interface between a cable and a connector is where most connectivity failures originate. Three failure modes are directly related to component matching:

Cable gland seal failure. The cable gland must compress the seal against the cable sheath—not the individual conductors and not the air around an undersized cable. When the cable outer diameter falls outside the gland’s sealing range by even 0.5mm, IP protection drops from IP68 to effectively IP00. LAPP’s SKINTOP® glands are dimensioned for ÖLFLEX® cable constructions, guaranteeing the seal compression that maintains rated IP protection.

Contact resistance increase. When a crimp contact is designed for a specific conductor construction (strand count, strand diameter, copper purity), the crimp creates a gas-tight joint with minimal resistance. Conductors from a different manufacturer may have different strand configurations, leading to higher contact resistance and heat generation under load.

Strain relief inadequacy. Cable weight, vibration and thermal cycling place mechanical stress on the termination point. Strain relief designs account for specific cable stiffness and outer diameter. When a cable is stiffer or heavier than the connector’s strain relief was designed for, the termination point bears excessive load—leading to intermittent faults that are difficult to diagnose.

These failure modes don’t appear on datasheets. They emerge during operation, often months after installation, when fixing them costs far more than specifying matched components from the start.

LAPP’s integrated portfolio: from cables to connectors to assemblies

LAPP engineers and produces every component in the connectivity chain:

ÖLFLEX® cables. Power, control, servo, data and instrumentation cables for every industrial application. From flexible drag chain cables rated for millions of flex cycles to static installation cables for permanent wiring. Available through the JJ-LAPP eShop with regional stock across ASEAN.

EPIC® connectors. Rectangular, circular, modular and solar connectors covering power transmission up to 250A, signal up to 280 contacts and data through Cat.6A Ethernet. Over 1,800 variants with UL, CSA and VDE certifications. EPIC® connectors are manufactured at LAPP Connector Dongguan (LCD)—LAPP’s dedicated connector production facility.

SKINTOP® cable glands. Over 8,000 variants from IP65 to IP69 in polyamide, nickel-plated brass and 316L stainless steel. Metric, PG and NPT threads with EMC shielding options.

FLEXIMARK® labelling. DIN EN 60204-1 compliant marking systems with UV-resistant printing for permanent cable identification.

ÖLFLEX® CONNECT assemblies. When your application requires pre-assembled connectivity, LAPP builds factory-tested cable harnesses using matched ÖLFLEX® cables and EPIC® connectors. Every assembly is 100% electrically tested before shipping—reducing your commissioning time by up to 40% compared to field assembly.

This portfolio means you can specify cables, connectors, glands, labels and pre-assembled harnesses from LAPP—with every component engineered to work with every other component in the range.

How do you evaluate a single-source connectivity partner?

Not every supplier claiming “single source” actually manufactures all components in-house. Many resell third-party connectors under their own brand. When evaluating a connectivity partner, ask five questions:

1. Do you manufacture both cables and connectors? LAPP manufactures ÖLFLEX® cables in multiple facilities globally and EPIC® connectors at LCD (LAPP Connector Dongguan). This is in-house manufacturing, not rebranding.

2. Are your components designed to work together? LAPP’s cable and connector engineering teams collaborate on specifications—cable outer diameters match gland ranges, conductor constructions match crimp specifications and sheath materials are compatible with connector seals.

3. Can you provide a single warranty covering both cable and connector? LAPP’s warranty covers the complete connection when LAPP cables and connectors are used together. No cross-supplier exclusions.

4. Do you offer pre-assembled solutions? ÖLFLEX® CONNECT harnesses demonstrate that LAPP’s cables and connectors are proven to work together—factory-assembled and 100% tested.

5. Do you have local technical support in my region? LAPP provides application engineering support through JJ-LAPP across ASEAN—covering cable selection, connector specification and assembly design in one conversation.

Talk to our engineers

LAPP’s application engineers help you evaluate the business case for supplier consolidation. They assess your current cable and connector specifications, identify compatibility risks in your existing multi-vendor setup and recommend integrated solutions that reduce procurement complexity while improving connection reliability.

Explore the full ÖLFLEX® CONNECT pre-assembled cable range or browse the EPIC® connector portfolio on the JJ-LAPP eShop.

Whether you are specifying cables and connectors for a new machine platform or reviewing an existing multi-vendor setup, LAPP’s engineering team provides a single point of contact for the full connectivity chain. Contact the team to discuss your integrated connectivity requirements and receive a specification review for your next project.